FB#.LINEPITCH
Description
This parameter defines the line pitch for linear encoders in nm per line. Only used when using linear motor types. For Rotary Motors, see FB.ENCLINES.
Examples
Context
See Feedback Devices and FB#.MECHTYPE.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
nm/line |
|
Range |
1 to 4,294,967,295 |
|
Default Value |
20,000 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.